Commercial Distribution
As needs in the market change over the years, so do our products. We've adapted our boards to allow for more outgoing ways, more RCD protection, more metering and surge protection .
The Range
Quadro Evo
Full power electrical solution for commercial buildings
Quadro Evo is not just a switchboard – Meticulously designed and engineered, it embodied Hager's commitment to excellence, safety, and efficiency. The release of Quadro Evo marked a significant milestone, signalling Hager's official entry into higher power Distribution board solutions.

Invicta 3 TP&N
Invicta 3 Type B boards have been designed for safe and simple installation, with features to benefit both installer and end-user.
Take a look below to see all of the features we have designed in and how this is going to make installing a distribution board so much easier.
Invicta Type B Hybrid Distribution Board
With standard MCB / RCBO based Electrical Distribution boards being limited to a maximum circuit rating of 63A, our Hybrid Distribution board provides a compact solution for Electrical Distribution and sits somewhere between an MCCB Panelboard and a TP&N Distribution board.
Aimed primarily at small commercial building applications, the solution provides protection and control for a small number of outgoing circuits up to 125A, with the majority of circuits still manged via standard MCB’s / RCBO’s.

Metered Power & Lighting Board
Monitoring Power and light loads separately to create a better understanding of the where electricity is being consumed. The Hager Power and lighting boards employ dual channel meters and are supplied with the main incoming device pre-installed.
Our board is available as standard in a variety of configurations and sizes to suit most applications up to 24TP ways. A Tri-metered TPN board is also available as standard, where separate monitoring of Power, Lighting and Mechanical services loads is required.
Benefits
Case Studies | Commercial Distribution
Enjoyed what you read? Check out some more of our other case studies to see how we were able to provide an ideal electrical solution.
FAQ
-
What is a 3 Phase Distribution board?
A 3 phase distribution board is a type of electrical distribution board that is designed to manage and distribute electrical power in a three-phase electrical system. In a three-phase system, three separate electrical currents are generated, each with a phase offset of 120 degrees. This provides a more efficient and reliable source of power compared to a single-phase system, which only generates one electrical current. The 3 phase distribution board acts as a central hub for distributing electrical power from the incoming supply to various electrical loads within a building or facility. It typically includes circuit breakers, fuses, and protective devices to ensure the safety of the electrical system and its users. 3 phase distribution boards are commonly used in commercial and industrial settings, where there is a high demand for electrical power and a need for a more robust and reliable electrical system.
-
What is the difference between a switch board and a distribution board?
A switchboard and a distribution board refer to different components in an electrical system:
- A switchboard is a large, centralized control panel that houses the main electrical switchgear and protective devices, such as fuses and circuit breakers. The switchboard is responsible for controlling and distributing electrical power from the incoming supply to various electrical loads within a building or facility.
- A distribution board, on the other hand, is a smaller, decentralized electrical panel that is used to distribute electrical power to various sub-circuits within a building. It typically includes circuit breakers, fuses, and other protective devices that help to ensure the safety of the electrical system and its users.
In summary, a switchboard is a larger and more centralized electrical panel that is responsible for distributing electrical power to various sub-circuits, while a distribution board is a smaller electrical panel that is used to distribute power within a building or facility.
-
What are the different types of distribution boards Hager offer?
Hager offers a wide range of distribution boards to meet the needs of various applications. Some of the different types of distribution boards that Hager offers include:
- Single-phase distribution boards: designed for use in residential and small commercial applications where a single-phase electrical supply is used. - Three-phase distribution boards: designed for use in commercial and industrial applications where a three-phase electrical supply is used.
- Type A and Type B distribution boards: these are designed for use in applications where residual current devices (RCDs) are required. Type A distribution boards are used in applications where high sensitivity is required, while Type B distribution boards are used in applications where increased immunity to false tripping is required.
- Metal Clad Distribution Boards: these are designed for use in harsh environments and are manufactured from robust metal materials.
- Surface-mounted distribution boards: designed for easy installation in a variety of locations and are typically used in residential and small commercial applications.
- Flush-mounted distribution boards: designed for installation in a recess or behind a wall and are typically used in residential and commercial applications where a neat and discreet installation is required.
- Modular distribution boards: these are designed for easy installation and maintenance, and are typically used in commercial and industrial applications where flexibility is required.
Hager offers a range of other distribution boards, including outdoor distribution boards, low-voltage distribution boards, and distribution boards with integrated metering.
-
Where can I download a Hager Commercial Distribution Catalogue?
You can download the Hager Commercial Distribution Catalogue here to access the catalogue
-
Where can a commerical distribution board be installed?
A commercial distribution board can be installed in a variety of commercial and industrial buildings, including: office buildings, retail stores, warehouses, manufacturing facilities, hospitals, schools and universities, hotels and other hospitality facilities, shopping centers, government buildings, religious institutions...
In these buildings, the commercial distribution board is typically located in a dedicated electrical room or closet, near the main electrical service entrance, to facilitate the distribution of electrical power throughout the building.
It is important to note that the location of the commercial distribution board must comply with local building codes and electrical safety regulations to ensure the safety of the electrical installation and the building occupants.
-
Where can I find Hager Disitribution board data sheet?
You can find Hager distribution board data sheet by searching for the product in the search bar, clicking on the page and scrolling down where you will find a data sheet can be downloaded.
-
What is a TPN Distribution Board?
TPN distribution board stands for Three Phase Normal Distribution Board. It is a type of electrical distribution board that is designed to distribute and control three-phase electrical power to various parts of a building. This type of distribution board is commonly used in commercial, industrial and large residential buildings, where there is a higher demand for electrical power. TPN distribution boards typically contain main switches, circuit breakers, and outgoing ways for connecting individual circuits, and they comply with international safety standards such as IEC 61439. The three-phase electrical system provides a more efficient and balanced distribution of electrical power compared to single-phase systems, and it is capable of handling higher loads. (click here to see our TPN Boards)
-
Do Hager Distribution boards come with SPDs?
It depends on the specific model and configuration of the Hager distribution board. Some Hager distribution boards come with built-in Surge Protective Devices (SPDs), while others may require external SPDs to be added. It is best to check the product specifications or contact Hager customer service to confirm if a particular distribution board model comes with built-in SPDs or if external SPDs are required.
-
What are the advantages of Hager metering solutions?
Hager metering solutions are highly advantageous for several reasons. Firstly, they offer accurate and reliable measurement of energy consumption, enabling users to track and analyze energy usage and identify opportunities for optimization and cost savings. Hager meters are compatible with a variety of energy sources, including electricity, and can be used in residential, commercial, and industrial settings.
Hager metering solutions are also easy to install and use. Additionally, Hager's meters are designed to meet regulatory requirements and standards, ensuring compliance and safety. This is especially important in highly regulated industries such as utilities and healthcare.
Finally, Hager metering solutions support energy efficiency and cost-saving initiatives, enabling users to track and reduce energy consumption and associated costs. This is increasingly important as organizations seek to reduce their carbon footprint and meet sustainability goals.
In summary, Hager metering solutions offer accurate and reliable energy measurement, ease of installation and use, and the ability to support energy efficiency and cost-saving initiatives, while also meeting regulatory requirements and standards.