Klik Black Hide In Plain Sight
Discover how Klik Black provides an ideal solution for retail and commercial settings. This new addition to our lighting connection range offers installation and aesthetic benefits sought in open ceiling applications.
To get in touch with our Klik Key Account Manager click the button below.

Klik Black Lighting Connection | A Low Visibility Solution
Our new adÂdiÂtion to our LightÂing ConÂnecÂtion range, Klik Black, provides the inÂstallÂaÂtion and aesÂthetic beÂneÂfits that speÂcifiers are seekÂing in open ceilÂing apÂplicÂaÂtions. CapÂitÂalÂising on all the feaÂtures of the Klik 4 Range, Klik Black aims to ofÂfer conÂtractÂors with an exÂtenÂded apÂplicÂaÂtion range to conÂform to proÂject reÂquireÂments.
EsÂtabÂlished as a marÂket leader in plug and play lightÂing conÂnecÂtion, Hager has reÂcently launched Klik Black – an exÂtenÂsion to their staple lightÂing conÂnecÂtion range, Klik. While mirÂrorÂing all the feaÂtures and beÂneÂfits of Klik 4 Pin, Klik Black provides inÂstallers with a low visÂibÂilÂity soluÂtion that’s ideal for open or semi-open ceilÂing apÂplicÂaÂtions.
The new adÂdiÂtion ofÂfers inÂstallers and buildÂing manÂagers with a wider apÂplicÂaÂtion seÂlecÂtion to acÂcomÂmodÂate proÂject speÂcificÂaÂtions. Klik Black aims to blend seamÂlessly into dark setÂtings where darker products are used, thus hidÂing in plain sight.
“We freÂquently reÂceived reÂquests from our cusÂtomÂers that showed a strong need for a low visÂibÂilÂity lightÂing conÂnecÂtion sysÂtem. We listened to the needs of our cusÂtomÂers and deÂveloped a soluÂtion that inÂcorÂporÂated all the beÂneÂfits of our Klik range while also enÂcomÂpassing a design suited for open ceilÂing apÂplicÂaÂtions,” said Product ManÂager, John ApÂpleton.
Products inÂcluded in the Klik Black range:
•MarÂshalling boxes
•PlugÂgable ceilÂing roses
•Klik 4 pin plugs & sockÂets
•OcÂcuÂpancy sensors
Ideal for a comÂmerÂcial or reÂtail setÂting, Klik Black deÂlivÂers comÂpliÂance of the neÂcesÂsary BS StandÂards for lightÂing conÂnecÂtion and elecÂtrical safety. With its plugs, sockÂets, PCR, marÂshalling boxes and even its matchÂing sensors, Klik Black will not only save time on-site, but conÂtractÂors can reÂmain conÂfidÂent that they are inÂstalling a seÂcure and aesÂthetÂicÂally pleasÂing soluÂtion.
Klik Black products
Discover our low visibility solutions
Related case studies
Read about how our products were able to provide an ideal solution.
Get inspired and discover how you can use our electrical installations in your next project.
Have some questions?
Check out our FAQ section to answer some questions you may have.
-
What installation settings is best suited for the Klik Black range?
The Klik Black range from Hager is specifically designed with modern aesthetics and versatility in mind. It's best suited for installation settings where the visual appeal is a priority, such as contemporary commercial spaces, high-end residential properties, or any space looking for a sleek, minimalistic finish.
We've ensured that the Klik Black range complements the design intent of such environments, blending seamlessly while providing the reliability and functionality you'd expect from us. So, when aiming for an elegant and modern touch, the Klik Black range is your go-to choice. -
What are the key features and benefits of the Klik Black Lighting Connection, especially in open ceiling applications?
The Klik Black Lighting Connection system from Hager is a game-changer, especially for open ceiling applications. Some of its key features and benefits include:
- Aesthetic Appeal: In open ceiling designs, every component is visible. The Klik Black range offers a sleek, modern, and discreet design that naturally complements contemporary interiors, ensuring that the connections don't detract from the overall aesthetic.
- Quick Installation: At Hager, we understand the value of time. The Klik Black system allows for faster and more efficient installations, thanks to its plug-and-play design, reducing installation time significantly.
- Flexibility: The system is highly adaptable, making it ideal for various lighting configurations. This means as layouts change or evolve, adjustments can be made easily without a complete system overhaul.
- Safety: Safety is paramount for us. The Klik Black range provides secure connections, ensuring that installations are both safe and reliable.
- Integrated Solutions: The system is designed to work seamlessly with any other Hager products, offering a holistic solution for your lighting needs.
For open ceiling applications where aesthetics, efficiency, and reliability are crucial, the Klik Black Lighting Connection system stands out as the preferred choice. -
Which products are included in the Klik Black range, and how do they contribute to low visibility and aesthetic solutions for commercial or retail settings?
The Klik Black range from Hager encompasses a suite of lighting connection products tailored for modern settings. Within the range, you'll find:
- Plug-In Ceiling Roses: These allow for quick connections, and their discreet black design ensures they blend seamlessly with darker ceiling finishes common in many contemporary commercial or retail interiors.
- Lighting Connection & Control Plugs: Designed with aesthetics in mind, these plugs provide a minimal visual footprint. Their dark hue makes them almost imperceptible against most open ceiling designs.
- Distribution Blocks: These are particularly useful for settings where multiple connections are needed, and their compact and black design ensures they remain inconspicuous.
In commercial or retail environments, the ambiance is everything. With the Klik Black range, we at Hager have ensured that the functional elements of the lighting system don't interfere with the desired aesthetics. The dark and sleek designs of these components fade into the background, letting the beauty of the space and the illumination stand out. It's a blend of utility and style, serving the modern demands of architects and interior designers.