Sollysta
Wiring Accessories
Our Sollysta White Moulded, Decorative, Grid, IP66 and Metalclad wiring accessories provide a full package of solutions for any project.
Sollysta’s hallmark features run consistently throughout the range, including the unique neutral loop terminal on the switch, moulded cable lead ins, captive and backed off terminal screws and the patented three pin shutter mechanism on the sockets for additional safety.
Product Technology
Sollysta
Neutral Loop Terminal
For many years domestic lighting circuits have been connected using the three plate method where the loop terminal is at the ceiling rose.
Today, it is increasingly likely that there is a decorative light fitting or even downlighters fitted in place of a standard pendant. These fittings are rarely provided with a neutral loop terminal.
It has also become popular to make the loop connection at the switch. This has the advantage of the connections being accessible and at a more convenient working height.
However, this leaves the problem of terminating the neutral conductor. One solution is to connect the neutral to a connector block inside the wall box, which takes up extra space.
Our solution is the Sollysta light switch which has a unique neutral loop terminal, built in.

Unique Safety Shutters
One of the fundamental requirements of the BS 7671 Wiring
Regulations is to provide basic protection against electric shock.
Sollysta sockets have a unique patented shutter system that not only requires the earth pin to be inserted first, but the simultaneous insertion of the live and neutral pins as well, before the shutter mechanism is activated. This enhances safety by making it difficult to defeat the mechanism and therefore reducing the risk of electric shock.
Advantages of Sollysta
for installers
Across the range
Sollysta was designed from the start to be the easiest on the market to install. We've kept these hallmark
features across the range to ensure that no matter what you're installing, it's always a simple job.
Product range
Sollysta
White Moulded
The Sollysta White Moulded switch range is one of
the easiest on the market to install, and with the shallow back-projection more cabling space is offered.
Behind the faceplate, the terminals face in the same direction with lead-ins for wiring, backed off screws held captive to prevent loss, wire end stops and clear white labelling off a dark grey background.
The wall switches are also the market's first with a neutral loop terminal built into the accessory. This allows the installer to complete the loop connection in the switch instead of in the ceiling rose.

Sollysta
Decorative
The high-quality modern finishes that are available within
the Sollysta decorative range fit seamlessly into any
setting and come with all
the installation features of the white moulded variant such as a neutral loop
terminal, cable lead in’s and the three pin shutter mechanism.
Available in both raised and flat plate options, the range offers you the flexibility to follow the design cues within the building making them perfect for any application.

Download the Catalogue
-
Check out the full range of Sollysta wiring accessories along with our junction boxes and ceiling accessories.
pdf15.26 MB
Get Inspired
Discover in the case studies below, how our solutions were able to provide an ideal electrical solution for customers and installers.
Have a question?
Our team of experts are on hand and ready to answer any questions you may have.
FAQ
-
What Decorative finishes does Hager Sollysta come in?
Sollysta Decorative range consists of two popular finishes; Brushed Steel and Polished Steel. Both finishes are available in a white and black insert in both a super low profile flat-plate and a stylish raised-plate
-
What features and benefits come with installing Hager Wiring Accessories?
Sollysta’s hallmark features run consistently throughout the range, including the unique neutral loop terminal on the switch, moulded cable lead ins, captive and backed off terminal screws and the patented three pin shutter mechanism on the sockets for additional safety.
-
Where should a key switch socket be used?
A key Switch socket is ideal for communal areas in multi-residential buildings, hotel lobbies and student accommodation, the fish key switch function means power to the socket cannot be turned on/off without using the removable key, preventing unauthorised use.
-
Why are Sollysta Wiring Accessories (or sockets and switches) easy to install?
All terminals face the same direction and the screws are backed out within moulded lead-ins, guiding the screw driver and screw head.
-
What’s the difference between Single Pole and Double Pole sockets?
The entire Sollysta range are double pole. Single pole will only switch the Live connection, double pole will switch both Live and Neutral and therefore isolating the connected appliance. Overall making it a safer choice.
-
How do Sollysta sockets give additional benefits to the basic protection of electric shock as required by BS 7671 of the Wiring Regulations ?
Sollysta sockets have a unique patented shutter system that not only requires the earth pin to be inserted first, but the simultaneous insertion of the live and neutral pins as well, before the shutter mechanism is activated. This enhances safety by making it difficult to defeat the mechanism and therefore reducing the risk of electric shock.
-
Do hager offer a USB socket?
Yes, we offer Sollysta twin switched sockets incorporating a Type C USB port as well as a Type A, suitable for charging most portable electronic devices.
Sollysta USB sockets offer intelligent connection to allow any USB device to charge at high speed.